Energy efficiency distributed solutions
 
 
 
 
 
  
 
 
 
 
 

Energy Efficiency: a common concern!

Under the Kyoto Protocol, industrialised countries have agreed to reduce their collective emissions of greenhouse gases by 5.2% by 2012, based on the level of emissions for 1990. Today electricity is the major contributor to greenhouse gases. Up to 50% of CO2 emissions attributable to residential and commercial buildings is from electricity consumption. Moreover, as domestic appliances, computers and entertainment systems proliferate; and the use of other equipment such as air conditioning and ventilation systems increases, electricity consumption is rising disproportionately to other energy usage. And this trend is here to last unless we do something!

More

 
 
 

Make the most of your Energy !

 
 
 
 

 

Solutions for residential and small buildings
Residential EE solutions may save 10% to 40% electricity

Discover this market 

 
 

 

Solutions for medium and large buildings
Buildings Renovation can yield up to 30% energy savings

Discover this market 

 
 

 

Solutions for industry and infrastructure
Industry & infrastructure: an average facility can reduce consumption by 10 to 20%

Discover this market 

 
 
  
 

 
Distributor network expertise

      


Schneider-Electric today technologies

      


For you 30% energy saving is achievable with today technologies. Up to 40% of the potential savings for a motor system are realised by the Drives & Automation. Up to 30% of the potential for savings in a building lighting system can be realised via the lighting control system.